Hello NXP
I sent the CAN TX signal via the flexcan_encrypted_s32k144 example code.
However, in CANOE, the TX signal is not received normally.
- CANOE trace
- used SendCANData code
How can I receive the CAN TX signal normally in CANOE?
Thanks
Dear Petr Stancik
When 'fd_enable' is set to false in struct 'flexcan_data_info_t', CAN Msg is normally received by CANOE.
Must 'fd_enable' be set to true?
And then, if we set 'fd_enable' to false, should 'enable_brs' be set to false?
Thanks
Dear Petr Stancik
The answer is not well understood.
Using the example code, CAN Msg delivered from CANOE to EVB(RX) has been received normaly.
However, there is an error when sending Msg from EVB to CANOE.
I think since RX is received, the bit timing seems to be well setting between CANOE and EVB.
Below is a configuration picture of the problem.
Please correct me if I misunderstood your answer.
Thanks