Program not starting after power on

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program not starting after power on

ソリューションへジャンプ
340件の閲覧回数
peacefulcarrot
Contributor II

Hi,

Kind of a stupid question, but I can seem to find why this doesn't work.

I am using a S32K144W. When debugging everything works fine and I can develop my application. However, when I disconnect the debugger (JLink) and power cycle my board, nothing happens. Pressing the reset button doesn't work. The application doesn't start.

When I attach my debugger and start the gdb server, the application does run when pressing the reset button.

Can you provide any pointer to why this is and how to solve this problem?

Thanks!

1 解決策
293件の閲覧回数
peacefulcarrot
Contributor II

Hi @Senlent ,

Thanks for your reply.

After some more testing the issue seemed to be the fact that I went to VLPS power mode. No idea why it works when the debugging is connected.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
301件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@peacefulcarrot

I have encountered some similar problems, and the reason for the failure was that the clock did not run

properly.You can check if there is any problem with the clock configuration

0 件の賞賛
返信
294件の閲覧回数
peacefulcarrot
Contributor II

Hi @Senlent ,

Thanks for your reply.

After some more testing the issue seemed to be the fact that I went to VLPS power mode. No idea why it works when the debugging is connected.

0 件の賞賛
返信