Power supply from eva board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Power supply from eva board

1,157 次查看
pietroserao
Contributor II

Good morning i have some questions.

 

I'm using a FRDMPK 144-Q100 S32k144 Evaluation board.

1) Can this microcontroller works with a 3.3V supply voltage?

2) Can i set the 3,3 V VDD voltage only using the evaluation board, without using external power supply?

    There is some setup?

 

Thank you.

标签 (1)
0 项奖励
回复
2 回复数

992 次查看
allen_willson
NXP Employee
NXP Employee

Pietro,

Yes this MCU can operate down to 2.7V

There is an unpopulated jumper at J10 which can allow to select between 3.3V and 5.0V. You'll need to remove the R64 which is a zero-ohm jumper that directly connects 5.0V to the micro - this needs to be removed so you can make a selection for 3.3V

Schematic attached.

#schematic

0 项奖励
回复

992 次查看
pietroserao
Contributor II

Thank you so much.

0 项奖励
回复