Port_Example_S32K344 is not working on S32K3X4EVB-T172 Evaluation Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port_Example_S32K344 is not working on S32K3X4EVB-T172 Evaluation Board

4,274 Views
cranes
Contributor III

Hello, 

I am running the example Port_Example_S32K344 on S32K3X4EVB-T172 Evaluation Board RevB (700-53148 Rev X5). But it fails at Mcu_InitClock() in main().

Then I realize that the function is commented out. But the condition is MCU_INIT_CLOCK is not STD_ON. Actually it is set as STD_ON in Mcu_Cfg.h.

Why is it like this? Is there anything missed here?

Thanks!

Crane

0 Kudos
Reply
18 Replies

4,254 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

I replicated the steps you described in my EVB (S32K3X4EVB-T172 SCH-53148 Rev A, 700-53148 Rev X3), and the board does not present that behavior with the Port_Example_S32K344.

I do not have that board revision at this moment (I am looking to get one of them).

Could you help me test the Port_Example example of the S32K3_M27X Real-Time Drivers Version 3.0.0 P07? This is to validate if it is not a software problem.

 

B.R.

VaneB

0 Kudos
Reply

4,241 Views
cranes
Contributor III
Hi Vanessa,
I can do that. But I couldn't find S32K3_M27X Real-Time Drivers Version 3.0.0 P07. Only S32K3XX AUTOSAR 4.4 - R21-11 RTD 3.0.0 D2303 is in the list.
Try to find it from the list of available updates. Installed another package that supports S32K344, but it doesn't provide more option when opening a new example.
Can you advice how to find the example you mentioned?
Thanks!
Crane
0 Kudos
Reply

4,207 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

Can you advise where he can find the example you mentioned?

The update package for S32DS can be downloaded from S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M -> S32K3_M27X Real-Time Drivers Version 3.0.0 P07 -> SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip or SW32K3_RTD_R21-11_3.0.0_P07_D2306.exe.

Once you download the updatesite.zip, open in S32DS the S32DS Extensions and Updates -> Add Update Site and select the package downloaded before. If it was correctly added in S32DS Extensions and Updates you are going to see an available update for the S32K3 RTD Autosar R21-11 Version 3.0.0. Once de update is done you should be able to create a project from an example of the S32K3_M27X Real-Time Drivers Version 3.0.0 P07.

VaneB_0-1698272156948.png

 

0 Kudos
Reply

4,199 Views
cranes
Contributor III

Tried and got the same result as before.

Regards,

Crane

0 Kudos
Reply

4,182 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

Do you mean that S32DS continues not to provide more options when opening a new example? Or does the code still fail on the clock initialization?

0 Kudos
Reply

4,172 Views
cranes
Contributor III

Hi Vanessa,

Sorry for the confusion.

Yes, I tried the new example in the updated version and still failed at Mcu_InitClock().

But it still looks like a software issue as the function Mcu_InitClock() definition should not be greyed out.

Regards,

Crane

 

0 Kudos
Reply

4,165 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

There is a possibility that the error is caused by package compatibility. To verify, please check if the package versions are the same as shown in the image. If it is not the same, please delete S32DS and reinstall it with the latest versions of the packages (S32K3_M27X Real-Time Drivers Version 3.0.0 P07, S32 Design Studio 3.5.6 Development Package with support for S32K3xx devices and others).

VaneB_0-1698357619606.png

0 Kudos
Reply

4,159 Views
cranes
Contributor III

cranes_0-1698358828969.png

This is from my computer. The version numbers look the same as yours.  Does it mean they are compatible?

0 Kudos
Reply

4,124 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

I already tested the example code with an S32K3X4EVB-T172 Evaluation Board RevB, and it works without problems. 

VaneB_0-1698444607788.jpeg

Please delete S32DS and reinstall it just with the latest versions of the following packages: S32K3_M27X Real-Time Drivers Version 3.0.0 P07 and S32 Design Studio 3.5.6 Development Package with support for S32K3xx devices.

0 Kudos
Reply

4,026 Views
cranes
Contributor III

Hi Vanessa,

Uninstalled everything and reinstall S32DS and RTD only P07. The result is the same as before.

Here are what's in my computer. Can you help check if there is any difference with yours?

cranes_0-1698679987440.png

cranes_2-1698680212571.png

cranes_4-1698680330269.png

cranes_10-1698680972684.png

cranes_6-1698680620587.png

cranes_7-1698680689095.png

Or anything else to compare to find the cause of the different result?

Thanks!

Crane

 

 

0 Kudos
Reply

3,987 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

If you test another example as Dio or any other, do you have the same behavior?

Also, are you using an external debugger or OpenSDA to program the MCU?

 

0 Kudos
Reply

3,984 Views
cranes
Contributor III

Hi Vanessa,

Tried Dio, Uart and PWM and only PWM works fine.

It looks as long as it is using Mcu_InitClock(), it gets stuck there. The function Mcu_InitClock() is greyed out.

I am using the debugger on the board, should be OpenSDA.

Regards,

Crane

 

0 Kudos
Reply

3,932 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

Do you have another board where you can validate if it has the same behavior?

Also, could you provide the exact number of silicon of the S32K344 of your board?

0 Kudos
Reply

3,927 Views
cranes
Contributor III

Hi Vanessa,

No, this is the only board I have.

What is the number of silicon? 

The exact number of the top is

P32K344EHVPBS

OP55A

CTZW2213A.

I have a question. Why is the definition of the function Mcu_InitClock() grayed out? It can't be found but it is called in Main().

Thanks,

Crane

0 Kudos
Reply

3,825 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

I apologize for the long time this is taking and for any inconvenience this may cause. 

I am still unable to replicate the behavior you are having with the EVB. I consulted with the internal team, and they are not able to replicate this situation. 

The example does not require any modification to work, so the definition of the function Mcu_InitClock() grayed out should not represent any problem.

Could you help me validate that the jumper configuration is the same as the Getting Started with the S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose?

Also, could you share an image of the HardFault given by S32DS?

0 Kudos
Reply

3,660 Views
cranes
Contributor III

Hi Vanessa,

Thank you for spending time on it.

Yes, the jumpers are the same as in the webpage you shared.

cranes_1-1700511461495.png

Other than changing the package from BGA257 to MQFP172, I didn't change anything else.

Here is how it goes when the program runs "step over" at the function Mcu_InitClock() .

cranes_0-1700511344680.png

Then if I click "View Disassembly", I see this:

cranes_7-1700512574895.png

This is how it goes if I just click run. 

cranes_4-1700511826283.png

Then if I click "View Disassembly", I see this:

cranes_2-1700511686761.png

If I click "Edit Source Lookup Path", I see this:

cranes_3-1700511779423.png

Yesterday I tried FreeRTOS LED example and it works fine as well. It doesn't call Mcu_InitClock() either. It looks not a must to call this function, is it correct? I haven't found the answer yet.

Today, I don't see the definition of Mcu_InitClock() is grayed out (I have no idea why). But when running "step into" at this function, the result is the same as running "step over". It doesn't goes into this function.

Thanks!

Crane

 

 

 

 

 

 

0 Kudos
Reply

3,644 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @cranes 

To verify that this behavior is not caused by a hardware problem, please test the Mcu_Example_S32K344 or the Clock_Ip_Example_S32K344. 

If you have a hard fault, try changing the example to use the internal clock. 

0 Kudos
Reply

3,638 Views
cranes
Contributor III

Hi Vanessa,

There is no problem running Clock_ip_example.

Tried to change the clock in Port_Example to FIRC and disable PLL. It seems not working with these error and warning:

cranes_0-1700611291930.png

Thanks!

Crane

 

0 Kudos
Reply