Dear All,
I am looking to determine the precise periodic frequency of the LPIT peripheral when operating in Compare Mode. Unfortunately, Figure 46-5 on p1392 (Rev 8. 06/2018) does not show the sequence in sufficient detail.
In short, my question is which formula is correct?
f_periodic = f_peripheral / (TVAL);
or
f_periodic = f_peripheral / (TVAL + 1);
The cook-book example ("hello_interrupts") suggests the first version since is specifies a divider of 40000000:
void LPIT0_init (void) { PCC->PCCn[PCC_LPIT_INDEX] = PCC_PCCn_PCS(6); /* Clock src=6 (SPLL2_DIV2_CLK)*/ PCC->PCCn[PCC_LPIT_INDEX] |= PCC_PCCn_CGC_MASK; /* Enable clk to LPIT0 regs */ LPIT0->MCR = 0x00000001; /* DBG_EN-0: Timer chans stop in Debug mode */ /* DOZE_EN=0: Timer chans are stopped in DOZE mode */ /* SW_RST=0: SW reset does not reset timer chans, regs */ /* M_CEN=1: enable module clk (allows writing other LPIT0 regs)*/ LPIT0->MIER = 0x00000001; /* TIE0=1: Timer Interrupt Enabled fot Chan 0 */ LPIT0->TMR[0].TVAL = 40000000; /* Chan 0 Timeout period: 40M clocks */ LPIT0->TMR[0].TCTRL = 0x00000001; /* T_EN=1: Timer channel is enabled */ /* CHAIN=0: channel chaining is disabled */ /* MODE=0: 32 periodic counter mode */ /* TSOT=0: Timer decrements immediately based on restart */ /* TSOI=0: Timer does not stop after timeout */ /* TROT=0 Timer will not reload on trigger */ /* TRG_src=0: External trigger soruce */ /* TRG_SEL=0: Timer chan 0 trigger source is selected*/ }
However, the reference manual says the TVAL value is loaded when the timer reaches zero. So, if the peripheral spends a full clock at zero value, then the periodic value in the example is slightly wrong since there are (TVAL+1) clocks per interrupt.
This will matter more when the timer values are short (e.g. TVAL = 100), where it would result in a timing error of roughly 1%.
解決済! 解決策の投稿を見る。
Hello Damien,
The first one is correct.
When it reaches 0, TVAL is loaded immediately.
..., 3, 2, 1, 0 (TVAL), TVAL - 1, ...
Regards,
Daniel
Hello Damien,
The first one is correct.
When it reaches 0, TVAL is loaded immediately.
..., 3, 2, 1, 0 (TVAL), TVAL - 1, ...
Regards,
Daniel