ON the Fly CAN baud rate change requirement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ON the Fly CAN baud rate change requirement

679 Views
vineet_gahlyan
Contributor I

Hi,

we are using s32k148 Nxp controller . we have  a requirement in which CAN baud rate should change on the fly without reset or power cycle.

Once baud rate is set then  we are not able to change the baud rate again without reboot.

We are able to set baud rate only  once in a power cycle.

 

But currently if we have set 500kb baud rate then we are not allowed to set 250 kb baud rate without reset or power cycle.

 Could  anyone help us to handle this situation... or is this s32k148 limitation??

1 Reply

597 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the FlexCAN module is in Freeze mode, then you can reconfigure bit timing register normally.

Unless you have CBT[BTF] bit set, and you are trying to modify CTRL1 register. In this case PRESDIV, PROPSEG, PSEG1, PSEG2, and RJW fields of CTRL1 become read only.
The CAN bit timing variables (PRESDIV, PROPSEG, PSEG1, PSEG2, and RJW) can also be configured using the CBT register, which extends the range of all these variables. And the CBT should be used for PRESDIV, RJW, PSEG1, PSEG2, and PROPSEG fields setting if CAN FD is enabled.

BR, Petr