Not able to run CSE (Cryptographic Service Commands) on S32R274RM Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to run CSE (Cryptographic Service Commands) on S32R274RM Board

677 Views
MadharKhan
Contributor I

Hi,

I am using S32R247RM Board. I would like to implement CSE on Board.
But i found CSE peripheral is disabled, when i looked in trace.

I have gone through AN4234 and AN5418 Application Notes and i understood the Commands.
but when i tried to implement it, no CSE related command is executing on board.

I tried by giving CSE_INIT(0x15) command  but this is also not running.

Do i need to add something in Lauterbach file to enable and run CSE commands?

please suggest me something that i can do to enable CSE.

Thank you.

0 Kudos
Reply
1 Reply

662 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
Hi,
could you please confirm what is your part number? There are three configurations of the chip and only 'B' and 'S' configuration have CSE module.
See the datasheet, page 10, Table 2 and 3:
It's not necessary to enable the CSE. If you have the right part number, it should work without initialization.
Regards,
Lukas

 

0 Kudos
Reply