Max SPI, UART, I2C, I2S, Camera, LCD channels when I use Flex IO in S32K312

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max SPI, UART, I2C, I2S, Camera, LCD channels when I use Flex IO in S32K312

ソリューションへジャンプ
692件の閲覧回数
hdlee
Contributor II

S32K312 has 32 I/O pins, 8 timers, 8 shift registers and 16 bits in counter.

So, I have below several questions for you.

Please check and reply it to me.

 

Q1. Max SPI channels supported in S32K312 using Flex IO

I think that SPI needs 4 lines(CLK, CS, MOSI and MISO). 

Referring to below table1, max SPI channels  are 4 in SPI master(SPI leader) and SPI slave(SPI follower).

 

Q2. Max UART channels supported in S32K312 using Flex IO

I think that UART at least needs 2 lines(UART TXD, UART TXD).

Referring to below table 1, max UART channels are 4.

 

Q3. Max I2C channels supported in S32K312 using Flex IO

I think that I2C  needs 2 lines(SCL, SDA).

Referring to below table 1, max master I2C channels are 4. I2C slave is not supported using Flex IO

 

Q4. Max I2S channels supported in S32K312 using Flex IO

I think that I2S needs 4 lines(BCLK, LRCK, DATA IN, DATA OUT).

Referring to below table, max I2S channels are 4 in I2S mater(I2S leader) and max I2S channels are 2 in  I2S slave(I2S follower)

 

Q5. Max Camera interface channels supported in S32K312 using Flex IO

Referring to below table, max camera interface are 2 because 11 camera signals are used.

 

Q6. Max 8080 LCD interface channels supported in S32K312 using Flex IO

Referring to below table, max 8080 LCD interface are 2 because 12 LCD signals are used

hdlee_0-1697234739959.png

Table 1. FlexIO supported Table

 

Best Regards

Heedong Lee

 

タグ(2)
0 件の賞賛
返信
1 解決策
640件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@hdlee

The picture you provided is already make it very clear.

I checked it and your understanding is correct!

 

 

元の投稿で解決策を見る

1 返信
641件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@hdlee

The picture you provided is already make it very clear.

I checked it and your understanding is correct!