Hello @JRoberto
Thank you for your reply.
Where can I find the specification for the maximum current for VDD_HV_A/B?
In an earlier version of the datasheet [S32K3xx Data Sheet, Rev. 2, DraftA, 11/2020] there was the following table. New datasheet does not contain this table anymore.
If I understood your answer correctly, then I could get 200 mA from it when using only one pin. What actually, according to my understanding can not be possible.
If there is no information about the maximum output current of a GPIO, would it be possible to get the R_DSON from the push-pull stage of the GPIO?
Thank You!
Hi,
The maximum current for all ports is given on Table 22 on S32K3xx Data Sheet, Rev. 5.2, 10/2022 with the description of "Output high current total for all ports".
The RDSON is not typically given on this kind of technology but given a defined voltage and a defined current you could do a good guess regarding the RDSON [Table 21, S32K3xx Data Sheet, Rev. 5.2, 10/2022].
This can be done with the maximum low voltage and the minimum current that it supplies and using the ohm law you could get the resistance.
Again, this is just a good guess that could apply to a worst-case scenario.
Please, let us know if this information was helpful.
Hello @Arkadiy
There is no such a typical max current for a single IO Pin, the VDD_HV_A or VDD_HV_B is like a current source with a maximum output capability. The sum of each IO current should not exceed the max capability of the GPIO otherwise you would damage the current source.
I hope this information helps!