Hello, I have a question about MPU setting for S32K118.
I have a problem when settin RGDACC register.
In S32K-RM_rev12_1 manual, register fields are the following:
Now in my program I was trying to set M1PE bit but in the attacched file(S32K118.h) no reference to this bit is present. All the other #define usefull to set the other bits are present.
Any reason for which the following code is not present?
#define MPU_RGD_WORD2_M1PE_MASK 0x800u
#define MPU_RGD_WORD2_M1PE_SHIFT 11u
#define MPU_RGD_WORD2_M1PE_WIDTH 1u
#define MPU_RGD_WORD2_M1PE(x) (((uint32_t)(((uint32_t)(x))<<MPU_RGD_WORD2_M1PE_SHIFT))&MPU_RGD_WORD2_M1PE_MASK)
#define MPU_RGDAAC_M1PE_MASK 0x800u
#define MPU_RGDAAC_M1PE_SHIFT 11u
#define MPU_RGDAAC_M1PE_WIDTH 1u
#define MPU_RGDAAC_M1PE(x) (((uint32_t)(((uint32_t)(x))<<MPU_RGDAAC_M1PE_SHIFT))&MPU_RGDAAC_M1PE_MASK)
This code is present in S32K14x.h file.
Thanks a lot.
Hello,
At first, thank you for your report. I'm very sorry for the delay, I have reported this to the responsible team a few weeks ago. But I'm waiting for the feedback.
When I receive any information I will let you know.
Best regards,
Diana