Hello, i am using s32k142 microcontroller, and when i am controlling a motor (pwm, direction) the applicxation will be restarted all the time, and when i have seen the RCM register to know the reason for reset, LOCKUP bit is set, but what can be the cause for this
Thank you in advance.
Hello Daniel,
Now it goes to one of the handlers, and it is actually going to "HardFault_Handler", but there is no much information about it in the link you sent me, do you have any idea what "HardFault_Handler" means, or what can be the problem ?
Thank you
Hi @elb1,
This is explained in the document, and the example handles hard faults too:
https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447
BR, Daniel
Hello @elb1,
When the core detects a fault exception, it fetches the HardFault_Hander().
The exception is then escalated to Core Lockup if the core detects another exception during the fetching.
Therefore I would say there is no HardFault_Hander() in the project.
Refer to this document/example, you should be able to find the exception that causes the fault.
https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447
Regards,
Daniel
Hello Daniel, Thank you for your response.
I have added those fault_exception files and it worked fine the microcontroller is not reset and also the control of the motor is working perfectly.
But the problem is that i didn't do anything except adding handlers, so is the problem still there ? or i don't know, i have also put break points in all those handlers but it didn't went to anyone of them
Thank you
Hello, more updates:
it was working only when i have put application only (in debug mode), but when flashed it with bootloader i got again the same behavior, the mcu is restarting and the reason again is LOCKUP, it also didn't stop in any of the handlers, it will be stopped somewhere in
No source available for "0x7bcce0e6"
Hi @elb1,
ARM documentation states:
"The processor enters a lockup state if a fault occurs when executing the NMI or HardFault handlers."
It could be because the HardFault vector is not implemented, therefore, I recommended adding it to the project.
Regarding the bootloader, please make sure the VTOR address is correctly changed to the vector table of the application. And read the HardFault vector in the memory view to ensure it has the pointer to the handler.
Regards,
Daniel
Hello Daniel, thank you for your response,
The thing is even when i divide for example by zero, to see if one of the handlers will be triggered but nothing, i think i am not testing as i should. I also tested with example project that you have provided you take a look at my response, i have put a comment there.
https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447
Thank you so much, i appreciate your help
Hi @elb1,
I just replied to your comment there.
Can you test the division by 0 in a new empty project?
Don't forget to enable the division by 0 trap.
Can you attach your project here so that I can test it?
BR, Daniel
Hi, yes i have enabled the division by 0 trap
I actually have tested in hello_world project, and it is going to the "UsageFault_Handler".
It's really strange in my project it doesn't, do you have any idea why?
Ps.I am using an RTOS operating system in my project, but even if i didn't started nor initializing any task, it still doesn't go to the handler.
Thank you
Are the handlers define in the startup_S32K142.S file
Have you checked the vector table in the flash?
Does it point to the handlers?
Can you share the project?
Regards,
Daniel