MCSPTE1AK144 Development Kit Application Software ver.1.2 Build Project Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCSPTE1AK144 Development Kit Application Software ver.1.2 Build Project Error

Jump to solution
706 Views
Juraj_PANCIK
Contributor I

Dears, 

I tried to build project "MCSPTE1AK144_BLDC_6Step" in order to get  file for flashing of MCU (MCSPTE1AK144_BLDC_6Step.srec) in version MCSPTE1AK144 Development Kit Application Software 1.2.

In difference from version 1.1 I got in this build in ver.1.2 the error message (pls see attached file Error Message.jpg). The S32DS extension and updates is on attached picture 240311 S32 Desig StudioCapture.jpg. See also note bellow [1].

Before work I set parameetrs for LINIX motor by running SetMotor-LINIX_45ZWN24-40.bat. 

As I wrote - the build in version 1.1 is without problem. 

Thank you very much for your kindly help

Juraj, teacher & development eng in Schaeffler AG. 

 

[1]

- S32 Design Studio (S32DS) for ARM 2.2
- S32 Software Development Kit (SDK) for S32K1xx 3.0.3

- S32K14x_AMMCLIB_v1.1.35
- FreeMASTER 3.1.4.5

 

0 Kudos
Reply
1 Solution
677 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It looks you are missing gdflib.h

This is part of AMMCLIB. Set your library paths accordingly your files location in project settings.

Includes and also libraries paths.

petervlna_1-1710403861009.png

 

petervlna_0-1710403737524.png

Best regards,

Peter

 

View solution in original post

0 Kudos
Reply
2 Replies
678 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It looks you are missing gdflib.h

This is part of AMMCLIB. Set your library paths accordingly your files location in project settings.

Includes and also libraries paths.

petervlna_1-1710403861009.png

 

petervlna_0-1710403737524.png

Best regards,

Peter

 

0 Kudos
Reply
640 Views
Juraj_PANCIK
Contributor I

Hi Peter,

thank you very much for your reply. I'll try do it.

I want remark that project mentioned by my is  a part of delivery of SW for EvaKit from NXP ver.1.2.  and in  such way it should not contains such errors ( as a sample it should be "buildable " without additional effort). The ver 1.1 of SW for this EvaKIt  is OK - this ver.1.2 need additional efort as you wrote.

Thank again. Have a nice day. Juraj 

0 Kudos
Reply