KITFS85SKTEVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KITFS85SKTEVM

3,006件の閲覧回数
yavuzklcc
Contributor III

Hello everyone

While trying to program the FS8530 chip on the KITFS85SKTEVM board,I encounter an error,I get the error ABIST2 FAIL.And it gets stuck in INIT_SAFE mode.

What can be done?

Thx. 

0 件の賞賛
返信
18 返答(返信)

2,985件の閲覧回数
yavuzklcc
Contributor III

hata.png

Fault screen

0 件の賞賛
返信

2,989件の閲覧回数
yavuzklcc
Contributor III

When i send FS_OVUVREG_STATUS message (VCOREMON_UV bit is 1) ,under voltage fault is fixed,but abıst2 fault continue.

0 件の賞賛
返信

2,954件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If fixed the Vcore UV issue,without other issue the ABIST2 will PASS. 

 

0 件の賞賛
返信

2,949件の閲覧回数
yavuzklcc
Contributor III
Thanks for answer.
Yes,but VCore UV issue dont fixed.What could be the source of the problem ?
0 件の賞賛
返信

2,896件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can check the Vcore related circuit to verify it again,I attached the schematic for you review.

 

 

0 件の賞賛
返信

2,886件の閲覧回数
yavuzklcc
Contributor III

 At the same time, I apply these steps exactly. But when I send the message to exit DEBUG mode,

1-) all regulators power on and the

2-)all regulators power off and RESET pin blinks 3 times.

This cycle continues.Something seems to be going wrong.

Iam beginner, i will be glad if you help

 

hata3.png

0 件の賞賛
返信

2,861件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please follow up the app note for operating this SBC step by step.

Better for your test used the programmed chip by NXP you can order this part instead of blank part OTP by yourself.

After familiar with EVB then you can do OTP by yourself.

 

 

0 件の賞賛
返信

2,892件の閲覧回数
yavuzklcc
Contributor III
I checked the VCOREMON pin. It doesn't see any problem . It is connected with BUCK1.
0 件の賞賛
返信

2,947件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

did you test the Vcore in your board? does it match what you setting value?

If Vcore is good,ABIST2 will pass no issue.

 

0 件の賞賛
返信

2,930件の閲覧回数
yavuzklcc
Contributor III
I knows that there is no point where I can measure Vcore directly. When I measure BUCK1 it matches the value i set.
0 件の賞賛
返信

2,926件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Does any error show in the GUI OV/UV or others iteam after your fixed VCORE?

0 件の賞賛
返信

2,924件の閲覧回数
yavuzklcc
Contributor III

hata1.png

After opening the card I only see the VCORE UV issue. 

0 件の賞賛
返信

2,955件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If in the OTP just as below picture showed, in the ABIST1,you enable the monitor of  VCORE/VDDIO/VMONX by OTP, in the  ABIST2 can  monitor VCORE/VDDIO/VMON1234 ,any error the SBC will hang. especially for the VMONX the reference voltage is 0.8V.

guoweisun_0-1677029306599.png

 

 

 

0 件の賞賛
返信

2,989件の閲覧回数
yavuzklcc
Contributor III

Yes.SBC stuck in ABIST2 phase.

hata.png

0 件の賞賛
返信

2,999件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Or can you give some picture for your error?

 

0 件の賞賛
返信

3,002件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Do you mean the SBC stuck in ABIST2 phase when start up in your board?

 

 

0 件の賞賛
返信

2,986件の閲覧回数
yavuzklcc
Contributor III
Yes.SBC stuck in ABIST2 phase.When i sent FS_OVUVREG_STATUS (VCOREMON bits is 1),under voltage fault is fixed ,but ABIST2 fault still continue.i will share you picture fault screen.
0 件の賞賛
返信

2,975件の閲覧回数
yavuzklcc
Contributor III
I tried but nothing change.
0 件の賞賛
返信