Import ECC key into HSE FW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import ECC key into HSE FW

ソリューションへジャンプ
1,529件の閲覧回数
IAussman
Contributor III

Dear NXP community,

I'm currently trying to import ECC public key into HSE FW.

OpenSSL has generated the private and public key with ".pem" extension.

So my question is, how to convert this pem file into something that could be used for key import.

Thank you for your support.

Best regards,

 

0 件の賞賛
返信
1 解決策
1,436件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @IAussman 

0x04 is a prefix only which says that it's uncompressed format.

Regards,

Lukas

元の投稿で解決策を見る

5 返答(返信)
1,498件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @IAussman 

see please attached document.

Regards,

Lukas

1,447件の閲覧回数
IAussman
Contributor III

Hi @lukaszadrapa ,

Is there any reason why the first byte of the ECC public key has been removed in the code source ?

Thank you.

Best regards,

 

0 件の賞賛
返信
1,437件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @IAussman 

0x04 is a prefix only which says that it's uncompressed format.

Regards,

Lukas

1,476件の閲覧回数
IAussman
Contributor III
Hi @lukaszadrapa ,

Thank you for your rapid response. I've followed the instructions for generating the ECC key.

HSE FW reference manual says that we have to format the key catalog prior to any key provisioning. By doing so (format catalog), I got an error saying "operation is not allowed". In my code source LC= CUST_DEL, so I should have super user rights.

If I bypass the catalog formating, I'm also getting the same error on the key import (NOT_ALLOWED).

Do you have any suggestions ? Thank you.

Below the code:

Crypto_Init(NULL_PTR);

RetVal = Crypto_Exts_FormatKeyCatalogs();

Crypto_KeyElementSet(CryptoConf_CryptoKey_ECC_PublicKey, /* CryptoKeyId */
CryptoConf_CryptoKeyElement_CryptoKeyElement_ECC_Public, /* KeyElementId */
SEC_au8Ecc256PubKey, /*Ecc public key address */
ECC_PUB_KEY_SZ /* Ecc public key size */);
1,456件の閲覧回数
IAussman
Contributor III
Problem solved by setting Key_Owner to OWNER_CUST for NvmKeyCatalog, and Key Owner to OWNER_ANY for RamKeyCatalog.

Best regards,