We are configuring SPI using EBtresos tool autosar package RTD 3.0.0.0. There are two types of buffers that is configurable:- Internal buffer and External buffer.
1. Is this internal buffer an array defined by Spi driver files in our software? How is it different from a user defined array in terms of speed?
2. Which is better/efficient? IB or EB
3. For IB, we have to first write to the IB a user defined array using Spi_WriteIB and then do Spi_SyncTransmit....whereas in EB, we can , use Spi_SetupEB() to setup this user defined array as the buffer and do Spi_SyncTransmit to do sync transmission. Which is faster/better, i think Eb only.
4. pls tell the pros and cons of both
已解决! 转到解答。
Hi @Guna,
I guess it depends on the usecase.
The Quality Package provides the expected execution time though.
Hi @Guna,
IB is setup by the driver, whereas EB is setup by the application SW.
The RTD comes with Quality Package, where you can find RTD_SPI_ProfileReport.xlsx with the execution time of each API.
Regards,
Daniel
But in IB after we have set up the array we have to write it into IB using Spi_WriteIB, we cannot access the IB directly right? the same array we can setup as EB and and modify and Transmit the data?
So, logically EB is faster right?