Hello
I want to use Watchdog of S32K144,but it does not work.I don't change the watchdog registers WDOG->CS and WDOG->TOVAL so that the watchdog should be initially active.The reset value of register WDOG->CS is 10100110000000 and WDOG->TOVAL has the predefined value 1024 and WDOG->CNT always 0.
Then i found an aswer :The watchdog is disabled in system_S32K144.c file if DISABLE_WDOG macro is defined in system_S32K144.h header file.
I commented out code but no reset. Are there any additional settings ?
Hi,
If I change DISABLE_WDOG to 0 in system_S32K144.h, it works on my side.
It is indicated by LED D1, it flashes when the MCU resets.
Could you check LED D1?
Regards,
Daniel