How to get one project with S2K324

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get one project with S2K324

329 次查看
IvyGuo
Contributor III

How to get one project rather than a core0 project and core1 the other project,Is there a demo like this? 

0 项奖励
回复
3 回复数

272 次查看
IvyGuo
Contributor III

Sorry, my expression may have caused you misunderstandings; At present, S32K324 has two independent projects based on Core0 and Core1. I would like to confirm if there is a single project with two main functions in it, rather than having the customer maintain two projects.

0 项奖励
回复

261 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @IvyGuo 

Thank you for the clarification. The RTD versions 2.0.0, 2.0.1, 2.0.2, and 2.0.3 provide an example named "Platform_Multicore_SingleElf_S32K324" which shows the usage of the multicore feature with a single binary file on S32DS for S32K324 derivative.

0 项奖励
回复

316 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @IvyGuo 

We have available examples of the Inter-Platform Communication Framework (IPCF). Subsystem that enables applications, running on multiple homogenous or heterogenous processing cores, located on the same chip or different chips, running on different operating systems, to communicate over various transport interfaces.

You can download them from S32K3 Standard Software > Automotive SW - S32K3 - Inter-Platform Communication Framework.

 

B.R.

VaneB

0 项奖励
回复