Hi ,
i review the RM of S32K1, the MCU wake-up sources as below.
1)we can select any general I/O pin to enter the VLPS by using the software config, only need to reserve this I/O pins on the PCB board, my understanding is right or not.
2) These below wake-up resources can be entered VLPS normally through the general I/O pins reserved by me. my understanding is right or not.
Best regards.
Guofred
已解决! 转到解答。
yes, I think all ports which can be configured as GPIO ,should be able to be used as wake-up source.and there are no particularly recommended ports for you, all the same.
This table describled the wake-up sources of the Low-power mode,instead of entering the Low-power mode.
for example, If MCU is in VLPS mode ,you can wake up the MCU through Pin Interrupts.
In the hardware design, some application need to use an external switch, you can use the external swtich to wake up the MCU from all low-power mode.
like EWM module,which is disabled in STOP1 and VLPS,so can not wake up the MCU from STOP1 or VLPS mode.
BR!
Jim,
Hi @Senlent ,
Thanks for your help.
so we can use the pin interrupts function to wake-up the MCU, if the MCU entering the low power mode.
would you like to recommend which pin to use to wake up faster, or any pin is normal wake up .
they don't have any difference on hardware when we want to design this pin to wake up.
my understanding is right or not.
Best regards.
Guofred