How to config PDB in S32K144 using MCAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to config PDB in S32K144 using MCAL

Jump to solution
505 Views
wuxianlong
Contributor III

Hi,all

I can‘t find the way to config PDB to trigger ADC channel or group. Can you give me some information or suggestions, it is best to provide a hardware-triggered ADC demo.

* Autosar Version : 4.4.0
* Autosar Revision : ASR_REL_4_4_REV_0000
* Autosar Conf.Variant :
* SW Version : 1.0.1

BRs,
xianlong

0 Kudos
Reply
1 Solution
424 Views
Nhi_Nguyen
NXP Employee
NXP Employee

Hi wuxianlong,

PDB used as default for S32K14X, so, you can find the example with trigger source is SW that was attached in the package with the link path: SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples.

For trigger source is HW, you can use one of them through this parameter:

Nhi_Nguyen_0-1694613408970.png

I attached the example for this. Please refer it.

 

Best regards,

Nhi

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
425 Views
Nhi_Nguyen
NXP Employee
NXP Employee

Hi wuxianlong,

PDB used as default for S32K14X, so, you can find the example with trigger source is SW that was attached in the package with the link path: SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples.

For trigger source is HW, you can use one of them through this parameter:

Nhi_Nguyen_0-1694613408970.png

I attached the example for this. Please refer it.

 

Best regards,

Nhi

 

 

 

0 Kudos
Reply