How flash to S32K144EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How flash to S32K144EVB

1,710 次查看
bryan_hong
Senior Contributor I

I execute `unified_bootloader_demo_V2.1.exe` so I can find as below.

bryan_hong_0-1693202876619.png

then, I try to build `S32K144_CANFD_bootloader` so I make S32K144_CANFD_bootloader.elf

bryan_hong_1-1693203255698.png

For example, I want to execute application(or firmware) I modified when S32K144EVB power on.

1.

so, I want to know how to flash application(or firmware) to S32K144EVB on `S32 studio`

which type files (.bin or .elf) must be flashed to update application(or firmware) ?

2.

and S32K144_CANFD_bootloader be marked bold as below. what is mean?

bryan_hong_2-1693204604762.png

I would like to know how to change the bold project to another project.

if there exist document alike `user guide for S32 studio`, plz share the documents.

 

3. 

What is this `S32K144_CAN_user_config` foler ?

flash_api.bin/S32k144_App_CANFD.bin -> this files will be re-generated ? if so, how to generate this files?

ECUBUS_CANFD_uds.json --> What is this file used for?

thanks

Bryan

0 项奖励
回复
3 回复数

1,653 次查看
bryan_hong
Senior Contributor I

I found `HOWTO_download_separate_elf_srec_hex_file_to_microcontroller_using_S32_Design_Studio.pdf`

btw, Must I buy below to download elf file to S32K144EVB ?

bryan_hong_0-1693377955780.png

 

0 项奖励
回复

1,630 次查看
bryan_hong
Senior Contributor I

plz answer this question and below

3. 

What is this `S32K144_CAN_user_config` foler ?

flash_api.bin/S32k144_App_CANFD.bin -> this files will be re-generated ? if so, how to generate this files?

ECUBUS_CANFD_uds.json --> What is this file used for?

thanks

Bryan

0 项奖励
回复

1,665 次查看
bryan_hong
Senior Contributor I

Hi

If there are any update, plz comment 

0 项奖励
回复