Just like the title.
I want use LIN to transmit and recieve data, but not find the function yet.
Need assistance, and Thanks a lot.
解決済! 解決策の投稿を見る。
Hi,
you can refer to the SDK based example which is part of S32 Design Studio. Example shows the usage of the LIN driver in master/slave mode. See examples called lin_master_baremetal_s32K144 and lin_slave_baremetal_s32K144 of the latest SDK version (RTM SDK 3.0.0).
You can also find simple non-SDK LIN master example on https://community.nxp.com/message/1109015?commentID=1109015#comment-1109015
BR, Petr
Hi,
you can refer to the SDK based example which is part of S32 Design Studio. Example shows the usage of the LIN driver in master/slave mode. See examples called lin_master_baremetal_s32K144 and lin_slave_baremetal_s32K144 of the latest SDK version (RTM SDK 3.0.0).
You can also find simple non-SDK LIN master example on https://community.nxp.com/message/1109015?commentID=1109015#comment-1109015
BR, Petr
How could get the demo?
Please asist.
I use LIN_DRV_MasterSendHeader function, it works, it can recieve frame header at LIN-MONITOR, but the LIN_DRV_SendFrameData function not so . Code below:
Need assistance and thanks a lot.