The example project under the file"C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2022_03\SW32K3_RTD_4_4_2_0_0_D2203\Can_TS_T40D34M20I0R0\examples\EBT\Can_example_S32K344" need so much header. but the header is not exist,the most of the header are configure file. Or can I get a appnote for integrate a project.
Thanks
the examples in EBT folder runs on EB Tresos Software,
The examples in the S32DS folder can be run directly on the S32 Design Studio,
you can take a look at the readme.txt file on both folders to know more.
BR!
Jim,