Hi NXP Team
I am using S32k118 in my project, and as per my project requirement, I have to generate two different frequencies i.e. 50khz and 625Hz.
In S32118 only two FTM channels are available i.e. FTM0 and FTM1
FTM1 is used as Flextimer Modulus Counter and FTM0 is used as PWM generator.
Is it possible to generate both 50khz and 625hz PWM from FTM0?
Please suggest
thanks
It's not possible to generate different PWM frequencies under the same module base,
BR!
Jim,