Generate Different frequencies with Single FTM-PWM channel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generate Different frequencies with Single FTM-PWM channel

930 Views
Learner
Contributor III

Hi NXP Team

I am using S32k118 in my project, and as per my project requirement, I have to generate two different frequencies i.e. 50khz and 625Hz.
In S32118 only two FTM channels are available i.e. FTM0 and FTM1

FTM1 is used as Flextimer Modulus Counter and FTM0 is used as PWM generator.
Is it possible to generate both 50khz and 625hz PWM from FTM0?
Please suggest 
thanks 

 

Tags (2)
0 Kudos
Reply
1 Reply

915 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Learner

      It's not possible to generate different PWM frequencies under the same module base,

BR!

     Jim,