I am reading the manual, but I am a bit confused about the relationship between Mailbox and Message Buffers. Are they the same thing?
解決済! 解決策の投稿を見る。
理解的不对,
参考上一个回答图片中的内容,每个MB的大小是可以配置的,所有的MB处于RAM的一段连续空间,当你使用信箱的时候,你需要先选择MB的大小(16,24,40,72),当然这个大小和CAN标准有关(CAN2.0或者CAN FD)。如果配置为FIFO,又有些区别。
Hi@symplesky
S32K-RM 55.5 Functional description:
The mailbox system is composed of a set of message buffers (MB) that store configuration and control data, time stamp, message ID, and data (see Message buffer structure).
Message Buffer Structure.
BR!
Jim.
Thank you for your reply, Jim. There are totally 32 Message Buffers in CAN1, when I set the Mailbox number with 16, dose it means every Mailbox have 2 Message Buffers?
理解的不对,
参考上一个回答图片中的内容,每个MB的大小是可以配置的,所有的MB处于RAM的一段连续空间,当你使用信箱的时候,你需要先选择MB的大小(16,24,40,72),当然这个大小和CAN标准有关(CAN2.0或者CAN FD)。如果配置为FIFO,又有些区别。