FlexCAN_Ip_Example_S32K344 example is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCAN_Ip_Example_S32K344 example is not working

431 Views
Coco_xie
Contributor II

Hello,

I am trying to run the FlexCAN_Ip_Example_S32K344 example on  NXP S32K3X4EVB-T172 but it not working.

I am just running the example code as it is, so there should not be any problem. Why FlexCAN_Ip_Send is not working ? Please help me let it work.

 

Info:

Board: S32K3X4EVB-T172

MCU: 32K344HMS 1P55A

IDE:S32 Design Studio for S32 Platform v.3.5(Windows)

Connect pin:(J32 pin1 and pin2 (TJA1153)) or (J39 pin21 and pin24)(Reference S32K3X4EVB-T172 Evaluation Board – REV B Schematics)

 

By the way, I already see NXP community have similar problem (FlexCAN Not Transmitting on S32K3X4EVB-Q172) it use Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200 to solved. But it Test HW is S32K3444EVB-Q172, I am not sure it is applicable to S32K3X4EVB-T172?

0 Kudos
6 Replies

407 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Coco_xie

1.yes, you can refer to this demo which will be applicable to S32K3X4EVB-T172

2."FlexCAN_Ip_Example_S32K344"-> this demo runs on loop-back mode and didn't init TJA1153(TJA1143). 

0 Kudos

402 Views
Coco_xie
Contributor II

didn't init TJA1153. Is mean not init FlexCAN_0?(I tring to init FlexCAN_0, but it still not send data.)

Can you help me init TJA1153 on FlexCAN_Ip_Example_S32K344 example?

0 Kudos

398 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Coco_xie

You can refer to the demo in the link.
TJA1154 requires some special initialization before it can be used

 

0 Kudos

394 Views
Coco_xie
Contributor II

But I can't use S32 Design Studio for S32 Platform v.3.5 to use demo(when open .mex file will have error)
I need download S32DS3.4?

Coco_xie_0-1708676733295.png

 

 

0 Kudos

387 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Coco_xie

这个例程是基于RTD 2.0.0制作的,直接参考然后修改至你当前使用的RTD版本,如果你想直接运行那么你需要安装RTD 2.0.0。

其实这么麻烦的主要原因是板子上的CAN收发器TJA1153需要做一些特殊的初始化才能正常收发。

0 Kudos

378 Views
Coco_xie
Contributor II
那我再嘗試看看,謝謝你。
0 Kudos