Hello,
I am trying to run the FlexCAN_Ip_Example_S32K344 example on NXP S32K3X4EVB-T172 but it not working.
I am just running the example code as it is, so there should not be any problem. Why FlexCAN_Ip_Send is not working ? Please help me let it work.
Info:
Board: S32K3X4EVB-T172
MCU: 32K344HMS 1P55A
IDE:S32 Design Studio for S32 Platform v.3.5(Windows)
Connect pin:(J32 pin1 and pin2 (TJA1153)) or (J39 pin21 and pin24)(Reference S32K3X4EVB-T172 Evaluation Board – REV B Schematics)
By the way, I already see NXP community have similar problem (FlexCAN Not Transmitting on S32K3X4EVB-Q172) it use Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200 to solved. But it Test HW is S32K3444EVB-Q172, I am not sure it is applicable to S32K3X4EVB-T172?