Failed to run generator "Wdg_TS_T40D2M10I4R0_GeneratorId" (mode: "verify") in EB Tresos Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to run generator "Wdg_TS_T40D2M10I4R0_GeneratorId" (mode: "verify") in EB Tresos Studio

1,981 Views
ronakpatel84
Contributor I

Please give me solution if you have any idea about this error. I am not able to generate the Wdg Module properly. So please help me as soon as possible.

ronakpatel84_0-1672054231298.pngronakpatel84_1-1672054255944.png

ronakpatel84_2-1672054274125.png

 

0 Kudos
Reply
5 Replies

1,070 Views
AmitoYao
Contributor II

You should modify the gpt module.

The callback of the gpt channel referred by the wdg module should  be Wdg_Cbk_GptNotification0

0 Kudos
Reply

1,909 Views
Shreya_Dave
Contributor I

Facing the same issue. Reinstalled package and tried but still getting the same error. Please help us for this

0 Kudos
Reply

1,894 Views
cuongnguyenphu
NXP Employee
NXP Employee

Let's give me information about your install environment:
- EB Tresos version
- SW package installing
- Did you have valid license for your SW package?

0 Kudos
Reply

1,956 Views
cuongnguyenphu
NXP Employee
NXP Employee

@ronakpatel84 
I think this issue is because some changes in Wdg_Cfg.h makes EB Generator cannot verify this file anymore.
We faced this issues number of times and the solution is uninstall the whole package and install it again

0 Kudos
Reply

1,086 Views
zhaogang
Contributor I

Hi,do you have other solution? I tried uninstall and install the tresos and SDK, stll the problem exist.

0 Kudos
Reply