Dear NXPS:
Chip: S32K146
OS: without OS
Q: When the FLASH_DRV_EraseSector interface returns a value other than STATUS_SUCCESS, I want to call the FLASH_DRV_EraseSector interface again. How much time should pass between the two calls?
Solved! Go to Solution.
Hello @Gideon,
There is no delay required, it can be called again immediately.
If you need the time required to erase one sector, refer to the S32K1xx DS, Table 35. Flash command timing specifications for S32K14x series
Regards,
Daniel
Hello @Gideon,
There is no delay required, it can be called again immediately.
If you need the time required to erase one sector, refer to the S32K1xx DS, Table 35. Flash command timing specifications for S32K14x series
Regards,
Daniel