Error in Eb teros by using autosar mcal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in Eb teros by using autosar mcal

666 Views
Nazni
Contributor I

Hi ,

I am getting error during my configuration

1,3,5 snapshot- You can see the error,It is showing Gigabit is not exist,& If you will see 5th image,Its showing In output/Generated/input folder “eth” file is not present,Why its happening.

for 2 snapshot-Why its telling Post build not supported,I did all configuration in gpt.

for 4 snapshot-In error ,Its telling we have not set wd0g0,and notification,But as you can see I did RE_Wdg_Cbk in notification,Why its so.

for 6,7 snapshot,You can see error for presalar,But I already set It,But one point,How we can enable predefined value(Showing in grey in 7th image).

How can i resolve these error,Please h

1000035646.png

  •   1000035645.png

elp

1000035644.png

1000035643.png

1000035642.png

1000035641.png

1000035640.png

  

0 Kudos
Reply
3 Replies

473 Views
NamLee
NXP Employee
NXP Employee

Hi Nazni,

I see a lot of errors here, but overall i think it's because some nodes are lack of data/missing resources.

The reason of this is because it's not the correct version of RTD.

Please make sure to use the correct version RTD and also version of tools.

"I am working on  S32K1XX_MCAL_4.3_RTM_1.0.5" >> I saw your project using RTM 1.0.4, so please try this release

Design : Product Download : Files (flexnetoperations.com)

NamLe_0-1703501944387.png

Inside your project, .xdm files will be found and they contain information of the MCAL version that project uses, for me is S32K14X_MCAL4_3_RTM_1_0_1

NamLe_3-1703502500289.png

And the plugin of the installed package should have the same information.

NamLe_2-1703502307562.png

Are you possible to share your project or the .xdm configuration files for me?

So i can check it directly.

Thank you,

Nam.

 

 

 

0 Kudos
Reply

642 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Nazni 

it would be nice to mention which device and which MCAL or RTD you have exactly. Also upload readable pictures. The uploaded ones are too small.

Regards,

Lukas

0 Kudos
Reply

631 Views
Nazni
Contributor I

Hi ,

Thanks for the reply.

I am working on  S32K1XX_MCAL_4.3_RTM_1.0.5 MCAL  AUTOSAR 4.0 OS for S32K14x.

1.PNG2.PNG3.PNG4.PNG5.PNG6.PNG7.PNG9.PNG

0 Kudos
Reply