Enable DMA causes large fluctuations in touch sense

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable DMA causes large fluctuations in touch sense

2,814 Views
LijieDu
Contributor II

When triggering DMA, if the source address is in flash or RAM space, but the destination address is in a peripheral register, it will result in inaccurate capacitance collection for touch sense.

If the DMA destination address is in Flash or RAM, the above phenomenon will not occur.

 

Touch sense note see attatchment

 

0 Kudos
Reply
13 Replies

2,789 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @LijieDu,

What S32K part is it?

And which peripheral register do you mean?

There could be issues with the arbitration on the crossbar switch.

Do you use Fixed priority or Round robin?

 

Regards,

Daniel

0 Kudos
Reply

2,780 Views
LijieDu
Contributor II

Hi @danielmartynek 

Sorry for the late reply.

I use s32k118, and generate waveforms with different duty cycles through FTM PWM mechanism.

So I use DMA chnl2 to periodically update the FTMx->Controls [chnl]. CnV register of FTM.

DMA chnl0 and chnl1 are used to tx and rx in spi moudle.

And round robin arbitration is used for channel selection.

0 Kudos
Reply

2,770 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LijieDu,

The eDMA has its own arbitration control (CR[RECA]).

And there is arbitration on the crossbar switch too:

danielmartynek_0-1698048058580.png

have you set CBRR = 1.

 

BR, Daniel

 

0 Kudos
Reply

2,745 Views
LijieDu
Contributor II

Hi @danielmartynek 

 

I have set CBRR to 1, and it has no improvement.

屏幕截图 2023-10-24 101731.png

The left side of the figure shows the measured values when the DMA destination address is set to the peripheral register.

The right side of the figure shows the measured values when the DMA destination address is set to the RAM space.

Only difference is destination address.

 

 

0 Kudos
Reply

2,699 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Can you elaborate on the description of the image? What each graph means?

Anyway, regardless of the arbitration, the peripherals can be access either by the eDMA or the Core at a time. And this can cause issues if the core frequently access the peripherals.

Do you use the highest system clock frequency?

 

Thanks,

Daniel

0 Kudos
Reply

2,695 Views
LijieDu
Contributor II

Hi @danielmartynek 

 

SysClk is 48MHz.

DMA trigger frequency is about 30khz(trigger DMA function every 33us), duration is about 30ms when enable DMA transfer function.

The description of the image: 

LijieDu_0-1698219590962.png

 

 Picture above shows: Measured values when the DMA destination address is set to the peripheral register and DMA is triggered in real time. We can see that the values get from ADC is unstable.

 

LijieDu_2-1698219942937.png

 

Picture above shows: Measured values when the DMA destination address is set to the RAM space and DMA is triggered in real time. We can see that the values get from ADC is stable.

 

 

 

0 Kudos
Reply

2,690 Views
danielmartynek
NXP TechSupport
NXP TechSupport

I see, thank you.

Have you tried using a different pin for the PWM output?

danielmartynek_0-1698238228315.png

BR, Daniel

 

 

0 Kudos
Reply

2,673 Views
LijieDu
Contributor II

Hi @danielmartynek  

I can have a try.

 

More description in detail:

I use 7 ADC channels (ADC0_SE3/ADC0_SE5/ADC0_SE6/ADC0_SE9/ADC0_SE12/ADC0_SE13/ADC0_SE14) to sample touch sense key. Same problem occurs in every channel. 

0 Kudos
Reply

2,662 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LijieDu,

There can be two issues, and we have already touched on that.

 

  • Arbitration

The DMA concept cannot be exactly deterministic, becasue the Core and the eDMA access the same resources through the crossbar switch and the peripheral bridge.

Before the GPIO pins are switched to High-Z, the ADC sampling already starts (1) to removed any remaining charge in the ADC sample and hold capacitor.

danielmartynek_0-1698324828228.png

1. ADC is triggered

2. GPIO in HIGH-Z

X. Sample ends (pin disconnected from ADC), conversion starts

3. Converion ends

If the ADC is triggered (1) with some delay due to arbitration, the sample phase starts and ends in different poinst, and this leads to incorrect measurement.

 

Can you try with a longer Sample time?

Do you use DMA to trigger the ADC conversions too?

 

  • Crosstalk, EMC

The high freq. PWM signal should not be at a pin adjacent to the touch sense pins (and traces).

 

Regards,

Daniel

 

 

0 Kudos
Reply

2,649 Views
LijieDu
Contributor II

I have tried to use different pin to generate pwm.

it doesn't work.

I have tried to make sample time longer(make it 1us and 2us).

it doesn't work.

/(ㄒoㄒ)/~~

0 Kudos
Reply

2,569 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LijieDu,

Is the VREF voltage stable during the operations?

 

Regards,

Daniel

0 Kudos
Reply

2,653 Views
LijieDu
Contributor II

Hi @danielmartynek 

 

Can you try with a longer Sample time?

Yes, I can try.

Do you use DMA to trigger the ADC conversions too?

No, only in spi and pwm out.

 

I have been on a business trip these past two days, so I don't have time to try. I will test and provide feedback on the results as soon as possible.

0 Kudos
Reply

2,765 Views
LijieDu
Contributor II

Hi @danielmartynek

 

I didn't set the bit to 1.

I can have a try and give you feedback on the results later. 

0 Kudos
Reply