Hello,
I'm using S32K146EVB-Q144. And tried to check the output CAN signal using external CAN device (CANoe) but didn't succeed. I guess the baud rate mismatched. The setting of the CANoe was 500KB/s.
How can I know the baud rate of the signal the can_pal_s32k146 example output.
The CAN periferal configuration was defined in can_pal1.c file generated.
My assumption is the below
The clock source is selected as CAN_CLK_SOURCE_OSC. This is 4MHz (Extenral Cyristal Frequency / 2).
baud rate = 4MHz / ((7+1) + (4+1) + (1+1) + 1) = 4MHz/16 = 250KHz.
Is my assumption right?
And when enableFD = false, is dataBitrate ignored?
Any response will be appliciated. Thank you.
已解决! 转到解答。
Hi
The example uses an 8MHz crystal, you can check it out here:
Note that: SOSCDIV2_CLK/1=8MHz
If enableFD = false, dataBitrate is ignored.
The example documentation can be found in the S32 SDK documentation at Examples and Demos section. (<SDK_PATH>/doc/Start_Here.html)
Please note: Power on the board with external supply 12V (J16). This information can be found in :file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.3/doc/html_S32K146/can_pal_s32k146_gr...
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you Robin for the quick reply.
I got it! (I had thought the 8MHz would be divided by 2 because of the name of the clock "SOSCDIV2_CLK" before being input to the CAN peripheral).
And I was using only USB cable. Let me modify the HW. Let me try again. I need some more HW modification, next reply will be delay sorry.
Best regards,
Tsunokawa
Hi
The example uses an 8MHz crystal, you can check it out here:
Note that: SOSCDIV2_CLK/1=8MHz
If enableFD = false, dataBitrate is ignored.
The example documentation can be found in the S32 SDK documentation at Examples and Demos section. (<SDK_PATH>/doc/Start_Here.html)
Please note: Power on the board with external supply 12V (J16). This information can be found in :file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.3/doc/html_S32K146/can_pal_s32k146_gr...
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------