Can't use PEmicro debugger with S32K118EVB2-Q048

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't use PEmicro debugger with S32K118EVB2-Q048

跳至解决方案
3,744 次查看
newbie
Contributor II

Dear sirs,

  I got S32K118EVB2-Q048 from Digi-Key this week and tried to run sample application(hello_world_s32k118) with PEmicro debugger(built-in OpenSDA) to check if the EVB is fine. Things were not going well and got errors as PEmicro_connection_assistant.png

problem_occurred.png

Info of environment:

OS: Windows 10 21H1

S32 Design Studio for S32 Platform Version: 3.4

S32 Design Studio S32K1XX SDK RTM 4.0.2

SDA_info ( is it ok of wrong board name? 

sda_info.png

Windows Device Manager: device_manager.png

drive.png

EVB is powered by USB and 3 leds were all on(D1:red, D2/D3:green) after powered.

Could anyone give some suggestion for this issue ? Thanks in advance.

标记 (3)
0 项奖励
1 解答
3,711 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please try to use P&E Recovery Utility halt MCU by refer Recovering Cortex-M Microcontroller with a Power Glitch.

Please try power cycling your board until this operation is successful.png

J16(external power) can be used to power cycling your board.(connect Pin1-2 of J107)
After halt the MCU, you should be able to debug it.

Success. Processor halted..png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
8 回复数
3,664 次查看
seini
Contributor I

@newbiecinema hd Still facing same issue. Can't able to figure out.

0 项奖励
3,712 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please try to use P&E Recovery Utility halt MCU by refer Recovering Cortex-M Microcontroller with a Power Glitch.

Please try power cycling your board until this operation is successful.png

J16(external power) can be used to power cycling your board.(connect Pin1-2 of J107)
After halt the MCU, you should be able to debug it.

Success. Processor halted..png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
3,685 次查看
newbie
Contributor II

Dear Robin,

  Thanks for your prompt support and this method unbricks my EVB.

  BTW, it only works under MCU voltage 5v. (connect Pin2-3 of J10)

  If MCU voltage is set to 3.3v, P&E Recovery Utility would never halt the processor even EVB is unbricked now.  (It was shipped with Pin1-2 connected of J10)

  I don't know if this behavior is ok or there is still something abnormal of my EVB.

 

  best regards,

0 项奖励
3,625 次查看
newbie
Contributor II

 

@Robin_Shen  Do you have any comment about the different behavior of MCU voltage setting ?

Thank you.

0 项奖励
3,591 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I cannot reproduce the problem you mentioned here.
I am using S32K118EVB-Q064 SCH-29945 REV. B.
The Application Version is: 1.23
J10 pin1-2
J107 pin1-2
J104 pin1-2

Maybe you can try to update OpenSDA Firmware.(Pemicro_OpenSDA_Debug_MSD_Update_Apps_2020_05_12\MSD-DEBUG-S32K118EVB-Q064_Pemicro_v123.SDA)

Application Version is 1.23.png

0 项奖励
3,586 次查看
newbie
Contributor II

Dear Robin,

  Thanks for your prompt reply. I had updated firmware of OpenSDA to v1.23 but MCU voltage3.3v still didn't work.

SDA_INFO_123.png

My EVB is S32K118EVB2-Q048 (48pin)

EVB_v2.jpg

Is it the same with yours?  Thank you.

0 项奖励
3,569 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry. I did not notice that your board is different from mine. Currently I don’t have S32K118EVB2-Q048 (48pin), so I can’t test it.

From the schematic, there are some changes in the power supply part, which may be caused by the difference.

0 项奖励
3,561 次查看
newbie
Contributor II

@Robin_Shen  May I request the schematic of S32K118EVB2-Q048 you mentioned because I couldn't find it at NXP's web site. Thank you. 

0 项奖励