Can't use PEmicro debugger with S32K118EVB2-Q048

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't use PEmicro debugger with S32K118EVB2-Q048

Jump to solution
3,453 Views
newbie
Contributor II

Dear sirs,

  I got S32K118EVB2-Q048 from Digi-Key this week and tried to run sample application(hello_world_s32k118) with PEmicro debugger(built-in OpenSDA) to check if the EVB is fine. Things were not going well and got errors as PEmicro_connection_assistant.png

problem_occurred.png

Info of environment:

OS: Windows 10 21H1

S32 Design Studio for S32 Platform Version: 3.4

S32 Design Studio S32K1XX SDK RTM 4.0.2

SDA_info ( is it ok of wrong board name? 

sda_info.png

Windows Device Manager: device_manager.png

drive.png

EVB is powered by USB and 3 leds were all on(D1:red, D2/D3:green) after powered.

Could anyone give some suggestion for this issue ? Thanks in advance.

Tags (3)
0 Kudos
1 Solution
3,420 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please try to use P&E Recovery Utility halt MCU by refer Recovering Cortex-M Microcontroller with a Power Glitch.

Please try power cycling your board until this operation is successful.png

J16(external power) can be used to power cycling your board.(connect Pin1-2 of J107)
After halt the MCU, you should be able to debug it.

Success. Processor halted..png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
8 Replies
3,373 Views
seini
Contributor I

@newbiecinema hd Still facing same issue. Can't able to figure out.

0 Kudos
3,421 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please try to use P&E Recovery Utility halt MCU by refer Recovering Cortex-M Microcontroller with a Power Glitch.

Please try power cycling your board until this operation is successful.png

J16(external power) can be used to power cycling your board.(connect Pin1-2 of J107)
After halt the MCU, you should be able to debug it.

Success. Processor halted..png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
3,394 Views
newbie
Contributor II

Dear Robin,

  Thanks for your prompt support and this method unbricks my EVB.

  BTW, it only works under MCU voltage 5v. (connect Pin2-3 of J10)

  If MCU voltage is set to 3.3v, P&E Recovery Utility would never halt the processor even EVB is unbricked now.  (It was shipped with Pin1-2 connected of J10)

  I don't know if this behavior is ok or there is still something abnormal of my EVB.

 

  best regards,

0 Kudos
3,334 Views
newbie
Contributor II

 

@Robin_Shen  Do you have any comment about the different behavior of MCU voltage setting ?

Thank you.

0 Kudos
3,300 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I cannot reproduce the problem you mentioned here.
I am using S32K118EVB-Q064 SCH-29945 REV. B.
The Application Version is: 1.23
J10 pin1-2
J107 pin1-2
J104 pin1-2

Maybe you can try to update OpenSDA Firmware.(Pemicro_OpenSDA_Debug_MSD_Update_Apps_2020_05_12\MSD-DEBUG-S32K118EVB-Q064_Pemicro_v123.SDA)

Application Version is 1.23.png

0 Kudos
3,295 Views
newbie
Contributor II

Dear Robin,

  Thanks for your prompt reply. I had updated firmware of OpenSDA to v1.23 but MCU voltage3.3v still didn't work.

SDA_INFO_123.png

My EVB is S32K118EVB2-Q048 (48pin)

EVB_v2.jpg

Is it the same with yours?  Thank you.

0 Kudos
3,278 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry. I did not notice that your board is different from mine. Currently I don’t have S32K118EVB2-Q048 (48pin), so I can’t test it.

From the schematic, there are some changes in the power supply part, which may be caused by the difference.

0 Kudos
3,270 Views
newbie
Contributor II

@Robin_Shen  May I request the schematic of S32K118EVB2-Q048 you mentioned because I couldn't find it at NXP's web site. Thank you. 

0 Kudos