Dear Supporters,
We have GHS licenses, and we are purchasing S32K3 board (S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose | NXP Semiconductors).
I have a question that: Can we create a S32K3 project with GHS compiler toolchain, and flashing and debug by micro-USB cable in S32 DS IDE?
We are now cannot prepare TRACE32 or any debug probe at this time, so we need to confirm about this solution can work.
Thank you,
Tien Tran.
Hello,
I have a question that: Can we create a S32K3 project with GHS compiler toolchain, and flashing and debug by micro-USB cable in S32 DS IDE?
I am not sure if you express yourself correctly. So 2 scenarios below:
1. if you are asking if you can create projectr in GHS and compile it and burn to the kit. Then answer is yes.
2. If you are asking for compilation of kit example SW (from NXP) then you need gcc compiler (S32DS for example). So no GHS compilation is possible.
Best regards,
Peter
Dear @petervlna ,
I read this document from NXP: How to Install Green Hills compiler plug-in into S32 Design Studio (see attached file).
I followed and installed GHS toolchain for S32 DS, then created sample project for S32K344. I tried to compile and there is no issue occur.
Could you confirm this example?
Hello,
Yes, you can use it.
As I have replied in first post. For new project is OK.
To compile existing examples written for gcc compiler, it wont work cause of different syntax.
Best regards,
Peter
Hello,
Yes. The S32DS is build on eclipse. So GHS plugin for eclipse can be used.
Best regards,
Peter
Dear @petervlna
Thank you for your confirmation.
But I have one question related to PEMicro. Could you confirm we can use micro-USB cable to connect and debug our software as above example setting.
We tested it's OK with S32K144EVB, but now we need to use S32K3 board for our project development.
Note: We are purchasing s32k3x4evb-t172 board, not have device to test and confirm this debug method.
Thanks.
Tien Tran