S32DS CDT indexer get stucks when indexing and parsing a c file.
the debug log in the console is
Indexer: parsing \BCU_CODE\src\Cdd\CDD_Diag\CDD_Diag.c
Warning: NLS missing message: CdtProjectIndexerSettingsInitializer_set_description_to_project in: com.nxp.s32ds.ext.cdt.internal.validation.core.messages
Warning: NLS missing message: RefreshPolicyValidator_refresh_failed in: com.nxp.s32ds.ext.cdt.internal.validation.core.messages
then i adjust the vm size , and no waning output. but the indexer process still stucks, and the cpu load of s32ds is 20%+ (almost one cpu core)
any one can help?
Hi,
for huge project Eclipse (on which is S32DS based) can't handle Indexer very well. You can try to disable it in Windows -> Preferences or play a little bit with settings:
I am sorry that this is not the root cause. I changed the parameters before I post the issue.
further more, I have modified the VM arguments in s32ds.ini the increase the memory that coule be used.
but nothing works.