CAN communication on s32k148EVB-Q144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN communication on s32k148EVB-Q144

870 次查看
harish_cont41
Contributor I

hi Guys,

 

I have huge problem of setting up CAN communication with my PC. I have flashed flexcan_encrypted_s32k148 SDK example and when I press SW3 or SW4 buttons I do not observe any change in the color of the LEDs. When both the LEDs are pressed one after the other I observe the change in color of the YELLOW Led on s32k148evb-Q144 board. I do not observe anything on the CAN Peak-system tool whether there was any TX or RX transmissions happened. Please help as i need to get started with the CAN communication setup quickly. To clarify CANH and CANL are properly connected and external 12V is provided. What I need is the communication through PEAK-System tool so I can develop my code accordingly. Right now I do see BUSHEAVY when I transmit some messages like 01h through PEAK system tool.

 

 

0 项奖励
回复
1 回复

862 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi harish_cont41,

The example documentation can be found in the S32 SDK documentation at Examples and Demos section. (<SDK_PATH>/doc/Start_Here.html)

FlexCAN Encrypted.png
Please read the documentation of FlexCAN Encrypted first.
Then configure the PCAN-Pro according to the FlexCAN configuration:
CAN                      FD
Arbitration Phase  500Kbps
Data Phase          1000Kbps

After press SW3 and SW4, the PCAN-Pro will show the CAN message sent from S32K148EVB board 1.

PCAN-View flexcan_encrypted_s32k148.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复