In order to establish the communication in CAN1 with on-board Transceiver do I need do the below hardware change???
1. Connect a jumper from PTE4 to PTA12.
2. And another jumper from PTE5 to PTA13, is that correct ?
And
Kindly share, if we have any direct method without changing the hardware or connecting any jumpers to configure the CAN 1 to onboard Transceiver.
Regards
Abhijith
Hi@abhijithshankar
you should remove R137 & R136,these two resisters may affect the CAN_H & CAN_L voltage.
BR!
Jim,