CAN 1 not working in s32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN 1 not working in s32k144

821 Views
abhijithshankaren
Contributor I

In order to establish the communication in CAN1 with on-board Transceiver do I need do the below hardware change??? 
   1. Connect a jumper from PTE4 to PTA12.

   2. And another jumper from PTE5 to PTA13, is that correct ?
   

And 

Kindly share, if we have any direct method without changing the hardware or connecting any jumpers to configure the CAN 1 to onboard Transceiver.

Regards
Abhijith 

0 Kudos
Reply
1 Reply

805 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@abhijithshankaren

you should remove R137 & R136,these two resisters may affect the CAN_H & CAN_L voltage.

Senlent_0-1635735928177.png

BR!

     Jim,

0 Kudos
Reply