Abnormal power down causing the Dflash area ???????(S32K342 MCAL)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Abnormal power down causing the Dflash area ???????(S32K342 MCAL)

971 Views
WangBk
Contributor III

Hello Support:

When we were testing, there was a very small chance that it would occasionally cause abnormal Dflash data:

WangBk_0-1709209075326.png

We suspect that it was caused by the chip powering off while operating the Dflash

When powered on again,FLS will read Dflash data, it will trigger hardfault.

And the error cannot be corrected.

Is there any way to resolve this error?

 

S32K342

FEE:Fee_TS_T40D34M20I0R0

FLS:Fls_TS_T40D34M20I0R0

WangBk_1-1709209336008.png

 

BR

WangBk

 

 

 

0 Kudos
15 Replies

944 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @WangBk,

It can be resolved by reprogramming the DFlash, which requires erasing the whole sector.

The read instruction that cause the hardfault can be skipped:

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-C40-Ip-ECC-Fault-Skip-S32K312-DS34-RTD2211-...

The power supply can be monitored so that any flash operation can ba launched when the power supply is stable.

 

Regards,

Daniel

0 Kudos

600 Views
Oskar_Waldemarsson
Contributor I

Hi @danielmartynek,

I also has some issues with ECC faults in DFlash area leading to hard fault when reading. I tested your example and it seems to work. But, some additional questions thet perhaps you could answer:

1. Is there no other way of dealing with ECC faults other than trying to handle and escape the hard fault manually? I.e. is there no setting that can make the read instruction continue without triggering an exception?

2.  In your example HardFault_Handler code you assume that the fault instruction address (stored PC) is always 8 positions from the top of the stack. Why is this so? I noticed that depending on how you configure the compiler (GCC) optimization the function prologue sometimes push 2 registers and sometimes 4 registers to the stack, making the 8 position offset somewhat unreliable. How can this be mitigated in a reliable way?

 

Regards, 

Oskar

0 Kudos

597 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Oskar_Waldemarsson,

1.

danielmartynek_0-1711615972617.png

2.

Yes, it depends on local variables, for example.

 

Regards,

Daniel

 

 

 

0 Kudos

591 Views
Oskar_Waldemarsson
Contributor I

Thanks for the quick reply! The DERR_SUP bit seems to be what I was looking for. 

Regarding the population of the stack. Do you have any information on how the stack gets populated during an exception and why the fault instruction address should be expected to be at position 8?

0 Kudos

578 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Refer to the ARM documentation:

https://developer.arm.com/documentation/dui0646/c/The-Cortex-M7-Processor/Exception-model/Exception-...

Then it depends on the compiler.

 

Regards,

Dnaiel

 

0 Kudos

912 Views
WangBk
Contributor III

Hi Daniel:

    The Demo code can skip the hardfault, Is there any way to fix abnormal areas?

BR

Wangbk

0 Kudos

900 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @WangBk,

According to AN13388 S32K3 Memories Guide, the data flash can be over-programmed only when used with NXP approved FEE driver.

danielmartynek_0-1709650434906.png

Otherwise, the flash sector must be erased first.

 

Regards,

Daniel

 

0 Kudos

814 Views
WangBk
Contributor III
Hi Daniel:
We also want to know what is the reason for this problem? What are the situations? Can you give some examples?
BR
Wangbk
0 Kudos

809 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @WangBk,

The flash controller programs the data + its ECC checksum into the flash.

If the programming is interrupted by power loss, the operation is incomplete, the data and its ECC checksum might not match.

The power supply can be monitored, so that any flash operation can be launched only under stable power supply.

 

Regards,

Daniel

 

 

0 Kudos

805 Views
WangBk
Contributor III

Hi Daniel

I have another question:
I plan to create an ECC fault in the 0x10014000 area. Some data is written in the 0x10014000 area through the FEE module.

Case 1: The following function call cannot cause ECC failure:

	/* Unlock sector if needed */
	if (STATUS_C40_IP_SECTOR_PROTECTED == C40_Ip_GetLock(FLS_SECTOR_TEST))
	{
		C40_Ip_ClearLock(FLS_SECTOR_TEST, FLS_MASTER_ID);
	}

	/* Erase sector */
	C40_Ip_MainInterfaceSectorErase(FLS_SECTOR_TEST, FLS_MASTER_ID);
	do
	{
		C40Status = C40_Ip_MainInterfaceSectorEraseStatus();
	}
	while (STATUS_C40_IP_BUSY == C40Status);

	C40_Ip_MainInterfaceWrite(FLS_SECTOR_ADDR, FLS_BUF_SIZE, writeBuffer_1, FLS_MASTER_ID);
	while (STATUS_C40_IP_BUSY == C40_Ip_MainInterfaceWriteStatus());

	/* Write 2 */
	C40_Ip_MainInterfaceWrite(FLS_SECTOR_ADDR, FLS_BUF_SIZE, writeBuffer_2, FLS_MASTER_ID);
	while (STATUS_C40_IP_BUSY == C40_Ip_MainInterfaceWriteStatus());

	/* Read */
	read_status = C40_Ip_Read(FLS_SECTOR_ADDR, FLS_BUF_SIZE, readBuffer);

 

Case2: The following function call can cause ECC failure

	/* Unlock sector if needed */
	if (STATUS_C40_IP_SECTOR_PROTECTED == C40_Ip_GetLock(FLS_SECTOR_TEST))
	{
		C40_Ip_ClearLock(FLS_SECTOR_TEST, FLS_MASTER_ID);
	}

	/* Erase sector */
	C40_Ip_MainInterfaceSectorErase(FLS_SECTOR_TEST, FLS_MASTER_ID);
	do
	{
		C40Status = C40_Ip_MainInterfaceSectorEraseStatus();
	}
	while (STATUS_C40_IP_BUSY == C40Status);

	/* Unlock sector if needed */
	if (STATUS_C40_IP_SECTOR_PROTECTED == C40_Ip_GetLock(FLS_SECTOR_TEST))
	{
		C40_Ip_ClearLock(FLS_SECTOR_TEST, FLS_MASTER_ID);
	}

	/* Erase sector */
	C40_Ip_MainInterfaceSectorErase(FLS_SECTOR_TEST, FLS_MASTER_ID);
	do
	{
		C40Status = C40_Ip_MainInterfaceSectorEraseStatus();
	}
	while (STATUS_C40_IP_BUSY == C40Status);

	C40_Ip_MainInterfaceWrite(FLS_SECTOR_ADDR, FLS_BUF_SIZE, writeBuffer_1, FLS_MASTER_ID);
	while (STATUS_C40_IP_BUSY == C40_Ip_MainInterfaceWriteStatus());

	/* Write 2 */
	C40_Ip_MainInterfaceWrite(FLS_SECTOR_ADDR, FLS_BUF_SIZE, writeBuffer_2, FLS_MASTER_ID);
	while (STATUS_C40_IP_BUSY == C40_Ip_MainInterfaceWriteStatus());

	/* Read */
	read_status = C40_Ip_Read(FLS_SECTOR_ADDR, FLS_BUF_SIZE, readBuffer);

 

Case 2 performs an erasure operation before case 1.

/* Unlock sector if needed */
	if (STATUS_C40_IP_SECTOR_PROTECTED == C40_Ip_GetLock(FLS_SECTOR_TEST))
	{
		C40_Ip_ClearLock(FLS_SECTOR_TEST, FLS_MASTER_ID);
	}

	/* Erase sector */
	C40_Ip_MainInterfaceSectorErase(FLS_SECTOR_TEST, FLS_MASTER_ID);
	do
	{
		C40Status = C40_Ip_MainInterfaceSectorEraseStatus();
	}
	while (STATUS_C40_IP_BUSY == C40Status);

 

Why is it not easy to reproduce ECC failures when Fee data exists?

 

0 Kudos

769 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @WangBk,

Can you read the return status of each function call?

 

BR, Daniel

0 Kudos

757 Views
WangBk
Contributor III

The return values are all correct, otherwise the program will be stuck in while(). My question is that the dflash is in the erasing state, which seems to make it easier to reproduce ECC faults.

0 Kudos

748 Views
danielmartynek
NXP TechSupport
NXP TechSupport

You don't even read the return status of some function e.g. C40_Ip_MainInterfaceWrite()

And it would be stuck in the while loop if the status remained BUSY.

danielmartynek_0-1710837487851.png

 

Regards,

Daniel

0 Kudos

721 Views
WangBk
Contributor III
Hi Daniel
sorry, It is the function parameters in my test code that are inconsistent, which leads to inconsistent test results. There is no problem with the Demo code.

878 Views
WangBk
Contributor III
Hi Daniel
Thanks.
BR
Wangbk
0 Kudos