AD detection is not allowed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AD detection is not allowed

987件の閲覧回数
ywjack
Contributor III

The accuracy of the ADC is not accurate. I used the ADC0 channel 13 (PTC15) to detect the voltage. But I found that the 3.3V is the ADC value is 1023, (ten-bit resolution), but I detected 2.5V is the ADC value of 808, already The 0.1V is worse. What's even more strange is that the ADC value I detected for 0.5V is 78. This variation is already very large. Can help me check if my location problem or other problem, I will attach my code configuration

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

913件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello ywjack@126.com,

Is the ADC module calibrated?

Do you use an EVB or your custom board?

Please measure VREFH, VREFL voltage.

Thank you,

BR, Daniel

0 件の賞賛
返信