I am having FS32K148UJT0VLQT on my design. Most of my I/O interfaces are 5V, but RMII interface requires 3.3V. I wonder if I can supply 5V to FS32K148UJT0VLQT and level-shift only the RMII interface signals down to 3.3V. I assume with 5V supplies, the RMII signals will become 5V and I can simply level shift them to 3.3. But I am not sure if the FS32K148UJT0VLQT RMII circuitry can handle 5V internally. Not sure if this is a possible solution? Thanks.
已解决! 转到解答。
Hi
I think you can refer to the schematic of S32K148EVB-SCH-29644-RB, TXB0104 is used.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
I think you can refer to the schematic of S32K148EVB-SCH-29644-RB, TXB0104 is used.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------