Example S32K144 Flash RW simple

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K144 Flash RW simple

Example S32K144 Flash RW simple

********************************************************************************
* Detailed Description:
* This simple example shows how to force function to RAM memory in S32 Design
* Studio and how to perform flash functions (Erase flash sector and Program
* phrase command in this case).
*
* ------------------------------------------------------------------------------
* Test HW:         FRDM-S32K144
* MCU:             PS32K144HFVLL 0N77P
* Fsys:            default
* Debugger:        Lauterbach Trace32
* Target:          internal_FLASH
*
********************************************************************************

标签 (1)
附件
评论

You can explain FCCOB Number 1 -> number 2. How to determine to fill this field.

example i want write into last sector in Program flash. How to do it 

is there any documentation to understand the example?

In my application I want to write some date in to flash and read it back after a power cycle.

could you please point me to a specific example.

Kind regards

无评分
版本历史
最后更新:
‎09-26-2016 01:27 AM
更新人: