Example S32K116 FlexCAN PN STOP S32DS.ARM.2.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example S32K116 FlexCAN PN STOP S32DS.ARM.2.2

Example S32K116 FlexCAN PN STOP S32DS.ARM.2.2

********************************************************************************
 Detailed Description:

 Example shows how to use FlexCAN 0 Pretended networking mode to allow FlexCAN
 module to wake up MCU from STOP mode using SDK.
 Wake up by Timeout and wake up by Match events are enabled.
 Also pin interrupt can be used to exit STOP mode.

 So MCU enters STOP mode by pressing SW3 button.
 MCU exits STOP mode when one of following happens:
 - no CAN message comes in 8sec (CAN PN timeout event)
 - message with standard ID 0x554 or 0x555 comes (CAN PN match event)
 - SW2 button is pressed (PTC12 interrupt)

 In run mode blue LED is dimming and the rate is different for each wakeup event

 ------------------------------------------------------------------------------
 Test HW: S32K116EVB-Q48
 MCU: PS32K116LAM 0N96V
 Compiler: S32DS.ARM.2.2
 SDK release: S32SDK_S32K1xx_RTM_3.0.0
 Debugger: Lauterbach, OpenSDA
 Target: internal_FLASH

********************************************************************************

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎06-25-2020 05:05 AM
更新者: