hi, NXP:
when i use BSP36 on s32g274ardb2 device, I found that OP-TEE is not working properly, I checked and found that the "tee-supplicant" process is working properly, but when I executed the hello-world example program, I found that it was an error;I am running normally on BSP33?
One additional piece of information is that I opened HSE in the ATF code on BSP36:
HSE_ARGS = " \ HSE_SUPPORT=1 \ "
Why is this happening, do I need to do additional processing or is there an issue with my operation?
that is the BSP36 error information:
已解决! 转到解答。
Hi,
Could be treated as a bug, but it is more of a conflict between both HSE and OPTEE.
As for a patch, we understand that under BSP39.0 a solution may have been implemented, but there is nothing else available at this moment, we do apologize.
We can recommend contacting your local NXP FAE/representative, since they may have more information on this regard. Again, we do apologize.
Please, let us know.
Hi,
We understand that, at this moment, there is a situation with the usage of HSE+OPTEE, where OPTEE is not able to run, for what we understand, are the base examples.
Can you help us understand if not using HSE provides the expected outcome from OPTEE? We do apologize for the inconvenience.
Please, let us know.
Hi,
This has been run within the internal team to confirm the behavior it was happening. If you are able to run OPTEE without HSE, then the situation seems to be related to the one that the internal team has able to confirm.
We do apologize for the inconvenience.
Please, let us know.
Hi,
Could be treated as a bug, but it is more of a conflict between both HSE and OPTEE.
As for a patch, we understand that under BSP39.0 a solution may have been implemented, but there is nothing else available at this moment, we do apologize.
We can recommend contacting your local NXP FAE/representative, since they may have more information on this regard. Again, we do apologize.
Please, let us know.