s32g274aevb booting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32g274aevb booting

919 Views
bbbjj
Contributor I

actually there is sometimes issue like under log

BUT now the issue appear all times when i try to boot. 

what is the reason ??

bsp : binaries_auto_linux_bsp28.0_s32g274

 


U-Boot 2020.04+geef88755a7 (Mar 03 2021 - 07:18:34 +0000)

CPU: NXP S32G274A rev. 2.1.0
Reset cause: Power-On Reset
Model: NXP S32G2XX
Board: NXP S32G274A-EVB
DRAM: 3.5 GiB
CA53 core 1 running.
CA53 core 2 running.
CA53 core 3 running.
All (4) cores are up.
MMC: FSL_SDHC: 0
Loading Environment from MMC... OK
Using external clock for PCIe0
Configuring PCIe0 as RootComplex(x2)
Using external clock for PCIe1
Frequency 125Mhz configured for PCIe1
Configuring PCIe1 as SGMII [XPCS0 1G, XPCS1 OFF(PCIex1)]
PCIe0: Failed to get link up
Pcie0: LINK_DBG_1: 0x00000000, LINK_DBG_2: 0x00000800 (expected 0x000000d1)
DEBUG_R0: 0x000f0600, DEBUG_R1: 0x08200000
PCI: Failed autoconfig bar 20
PCI: Failed autoconfig bar 24
PCIe1: Not configuring PCIe, PHY not configured
In: serial
Out: serial
Err: serial
usb dr_mode not found
EHCI fail to reset
enable_saf1508bet: Cannot find USB device
initcall sequence 00000000fcfc8ca8 failed at call 00000000340a2f98 (err=-1)
### ERROR ### Please RESET the board ###

0 Kudos
Reply
2 Replies

598 Views
kamalakkannanna
Contributor I

Any update for the above issue, i am facing the same issue.Any missing part please let me know.

0 Kudos
Reply

841 Views
nxf92355
NXP Employee
NXP Employee

Hello

 

did any changes in u-boot ?  or on board ?

 

thanks

regrade

0 Kudos
Reply