interrupt buffer of function and #pragma data section

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

interrupt buffer of function and #pragma data section

2,057件の閲覧回数
InHome
Contributor III

Dear NXP Hello,

I want to store all the ISR functions in a buffer and affect the pointer to the INTC->IACKR0 register.

INTC->IACKR0  = (uint32_t) &Buffer[0];

But when I debug this line, IACKRO doesn't have the address, it has a part of the address.

I comprehend that I have to map this buffer to the .bss section interrupt but I don't know how to do this

may be like this but, I am not sure.

#pragma gcc section sbss=".intc_vector_table"

could confirm this or suggest how this could be done?

Thank you in advance,

Taha

 

0 件の賞賛
返信
1 返信

2,046件の閲覧回数
InHome
Contributor III