how to create sja1110_uc.bin and sja1110_switch.bin from S32DS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to create sja1110_uc.bin and sja1110_switch.bin from S32DS?

ソリューションへジャンプ
2,439件の閲覧回数
Simon666
Contributor II

I want to use SPI to download sja1110 firmware with different config and code base,

how to create a new image for sja1110 not only use GOLDVIP image?

thanks

タグ(1)
0 件の賞賛
返信
1 解決策
2,403件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Simon666,

You need to download the SJA1110-EVM Configuration Tools from: https://www.nxp.com/products/interfaces/ethernet-/automotive-ethernet-switches/sja1110-evm-evaluatio...

Is not only for goldvip image you can apply to your desing

https://www.nxp.com/document/guide/get-started-with-the-sja1110-evm:GS-SJA1110-EVM

 

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,404件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Simon666,

You need to download the SJA1110-EVM Configuration Tools from: https://www.nxp.com/products/interfaces/ethernet-/automotive-ethernet-switches/sja1110-evm-evaluatio...

Is not only for goldvip image you can apply to your desing

https://www.nxp.com/document/guide/get-started-with-the-sja1110-evm:GS-SJA1110-EVM

 

Regards

0 件の賞賛
返信
2,401件の閲覧回数
Simon666
Contributor II

I already download the SJA1110-EVM patch, but only get flash.bin, no other bin files, where is uc.bin and switch.bin?

0 件の賞賛
返信
2,100件の閲覧回数
Ethan_L
Contributor III

hi @Simon666 ,

Do you know how to create sja1110_switch.bin and sja1110_uc.bin, I have the same problem about this.

Thanks, Ethan.

1,608件の閲覧回数
Gerry15
Contributor III

Hey,

 

take a look at the following git repository of nxp.

If you want use the Linux BSP of NXP, it is possible to add the "sja1110" layer similar to the "pfe" layer, which will download the mentioned files from the git repo. Take a look at building the Linux BSP!

 

Greetings

 

0 件の賞賛
返信