how to create sja1110_uc.bin and sja1110_switch.bin from S32DS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to create sja1110_uc.bin and sja1110_switch.bin from S32DS?

Jump to solution
2,256 Views
Simon666
Contributor II

I want to use SPI to download sja1110 firmware with different config and code base,

how to create a new image for sja1110 not only use GOLDVIP image?

thanks

Tags (1)
0 Kudos
Reply
1 Solution
2,220 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Simon666,

You need to download the SJA1110-EVM Configuration Tools from: https://www.nxp.com/products/interfaces/ethernet-/automotive-ethernet-switches/sja1110-evm-evaluatio...

Is not only for goldvip image you can apply to your desing

https://www.nxp.com/document/guide/get-started-with-the-sja1110-evm:GS-SJA1110-EVM

 

Regards

View solution in original post

0 Kudos
Reply
4 Replies
2,221 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Simon666,

You need to download the SJA1110-EVM Configuration Tools from: https://www.nxp.com/products/interfaces/ethernet-/automotive-ethernet-switches/sja1110-evm-evaluatio...

Is not only for goldvip image you can apply to your desing

https://www.nxp.com/document/guide/get-started-with-the-sja1110-evm:GS-SJA1110-EVM

 

Regards

0 Kudos
Reply
2,218 Views
Simon666
Contributor II

I already download the SJA1110-EVM patch, but only get flash.bin, no other bin files, where is uc.bin and switch.bin?

0 Kudos
Reply
1,917 Views
Ethan_L
Contributor III

hi @Simon666 ,

Do you know how to create sja1110_switch.bin and sja1110_uc.bin, I have the same problem about this.

Thanks, Ethan.

1,425 Views
Gerry15
Contributor III

Hey,

 

take a look at the following git repository of nxp.

If you want use the Linux BSP of NXP, it is possible to add the "sja1110" layer similar to the "pfe" layer, which will download the mentioned files from the git repo. Take a look at building the Linux BSP!

 

Greetings

 

0 Kudos
Reply