debug qbv in sja1110

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

debug qbv in sja1110

307 次查看
cristianchacha
Contributor III

Hello,

I'm using a SJA1110 and Qbv configuration, I did some test and it seems from time to time qbv period is missing.

I using Qbv port 4 with period 20ms and the following scheduling
close gate = 8ms
open gate = 2ms
close gate = 200ns

the explanation of lasted gate short period is to avoid contraint time to compare clock for next period Qbv and actual gate time.

How can I analize deeper this issue with S32 DS tool? is there any counter for error or any kind to debug qbv performance ?

thanks in advance

0 项奖励
回复
0 回复数